2025-03-02 5:07 AM
Hello everyone,
I'm current creating my first STM32 design using STM32F411 and have a need for the USB function on the MCU. The datasheet states that it requires a 48 MHz clock generated by a PLL connected to the HSE oscillator.
And I've currently chosen the CSTNE8M00G520000R0 ceramic resonator by muRata with built in capacitors for HSE.
Now with my understanding of an2867, I need to calculate the external resistor value based on ESR for crystal based designs.
Based on this post, it seems that ceramic resonator require external resistor, too.
However, I couldn't seem to find the ESR or maximum DL value on the webpage or datasheet of the ceramic resonator.
So my question is if I need an external resistor, and if so, what value should be?
Sorry if I'm not clear enough and thanks in advance.
Solved! Go to Solution.
2025-03-02 8:52 AM
Dear @Timothee ,
Welcome in STCommunity !
If in your application USB is required , I do not recommend to use that Ceramic resonator as you can see it’s datasheet it has 0,5% of precision at initial state . USB requires 500 PPM maximum of precision, So I suggest to use standard quartz of 8 or 16 , 24 etc MHz .
You need to have CL1 and CL2 capacitors and without a need for Rext . Very rare saw at our customers design .
Hope it helps you .
Regards, STOne-32
2025-03-02 8:52 AM
Dear @Timothee ,
Welcome in STCommunity !
If in your application USB is required , I do not recommend to use that Ceramic resonator as you can see it’s datasheet it has 0,5% of precision at initial state . USB requires 500 PPM maximum of precision, So I suggest to use standard quartz of 8 or 16 , 24 etc MHz .
You need to have CL1 and CL2 capacitors and without a need for Rext . Very rare saw at our customers design .
Hope it helps you .
Regards, STOne-32
2025-03-03 5:07 AM
Understood, thanks for the quick response.