Solved
stm32f407vgt6 problem with UART
I have stm32f407vgt6 from devebox. At first, I wanted to do led blink and it worked fine when I supplied it with external power via 5V pins. Then, when I tried to use UART pin (PA_9, PA_10) to print something to USB to TTL module, it did nothing. UART pins only work when I connected micro USB on stm32f407vgt6. Does anyone know how to solve this?