2016-06-07 05:55 AM
Hi all, I try to understand break input.I read break input title in datasheet.Refer to ''The break functionprotects power switches driven by PWM signals generated with the advanced timers.'' in the datasheet. But I didn't understand power switches there.Which power switches? Can I only connect 3,3v or gnd to BKIN Pin(pA6).Can you give information briefly about it?Can you help me?
2016-06-07 06:02 AM
Motor control type applications, using external power control circuits (switches) supplying higher current / voltages
Break Input, providing a means to leave the PWM outputs to the external switches in a safe state2016-06-07 06:09 AM
Hi berk.ata,
I recommend you to have a look to the application note about STM32 device timer break feature -Syrine-2016-06-07 06:38 AM
I suppose ı understand.Briefly,Break input leave pwm outputs for hold harmless motors etc(power circuit..) İs that so?
http://tureng.com/tr/turkce-ingilizce/so%20what%20you%27re%20saying%20is
http://tureng.com/tr/turkce-ingilizce/so%20what%20you%27re%20saying%20is