cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407vg discovery stlinkv2 virtual com port for uart/usb

hackerli90
Associate II
Posted on October 31, 2017 at 11:54

hi. i work with the stm32f407vgDiscovery kit. i used the stm32f103rbNucleo kit before which has an stlink with a cirtual com port which i used with uart. the current board stm32f407vgdiscovery lists a virtual com port on my computer and i can also connect to it but i dont know how to use it. The schematics do not route the stlinkv2 to the boards uart nor usb. Is this not ment to be used ? There is an alternative to use cn5 (usb connector on board, not stlink) but id really prefer it to use the one within the stlink to have one cable only.

1 REPLY 1
Posted on October 31, 2017 at 13:58

The DISC1 version has an ST-LINK chip supporting the VCP, the circuit board wasn't updated so you'd have to wire the chip manually.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..