cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407IGT6 - SECTOR0 write problem

211607
Associate
Posted on May 13, 2013 at 09:35

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 13, 2013 at 14:54

What is the happen? Why I'm not able to use SECTOR0 at FLASH-memory?

Yes, well that does look rather odd, and the option bytes, at least from a skim of the manual look correct, ie Read Protection not protecting 0, and Write Protect not enabled on any.

Were you doing something with it prior to it getting in this state? Does cycling the power help?

Keil seems to be loading an older version of the DLL, might want to also double check if option bytes are included in the flash algorithm dialog. You could try a different JTAG pod, or see if there are any STM32 JLink tools in the Segger directory.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..