cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 Ethernet Error

younginpark
Associate II

The problem you are experiencing with your STM32F407IGT6 board is that after programming the firmware and using Ethernet (UDP) communication, if you power it off and then back on, the Ethernet communication doesn't work. However, if you press the Reset button, Ethernet communication becomes operational again. Do you happen to know the reason for this?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Could be getting stuck on startup in some initialization method, perhaps clock initialization. Instrument your code or attach a debugger without resetting to understand where the processor is at when it's stuck and correct.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

Could be getting stuck on startup in some initialization method, perhaps clock initialization. Instrument your code or attach a debugger without resetting to understand where the processor is at when it's stuck and correct.

If you feel a post has answered your question, please click "Accept as Solution".
younginpark
Associate II

When entering debugging mode and opening the "start" file, the main screen does not appear. In this state, it is only when you perform a restart (Run -> Restart) that it starts from the "Main.cv" file. Is there a possible connection with this issue? I'm also providing the code for your review. Can you help me investigate this?