2016-09-29 10:41 PM
STm32f407 problem in standby and wakeup
2016-09-29 11:13 PM
2016-09-30 02:23 AM
Hello,
To more understand your issue, we need more details about your application and configuration.- Which Cube version using ? - Are you using CubeMX generated code ?- Did you added your own code or used one of the firmware examples from the STM32Cube packages?Regards2016-10-03 01:49 AM
Sorry I posted from mobile phone but it does not work .
problem :
we use standbye mode ; we noticed that while the MCU in the standby mode and the
VDD is removed then the VDD is reconnected ( this can happened while replacing the battery during standby mode) ; the MCU never wakeup it needs an hardware reset to start again; and since this is not possible in our product because Reset is inside the pcb ; can you suggest a solution for our problem ; please ?
Thank you inadvanced
2016-10-04 07:16 AM
Any suggestion here friends ?
2023-10-08 10:32 PM
we are also facing the same issue now did you got any solution please share here. It is very helpful for us.