2021-01-05 7:34 AM
My data has zeros every 2 bytes.
it's like this: 0x55 0x55 00 00 0xaa 0xaa 00 00 0x33 0x33 00 00 ......
I want to remove these zeros with address increment feature of DMA.
I wrote a configuration for stm32f107 DMA and removed these zeros without problem but when I write same configuration for stm32f407 all data is copied.
my configuration is:
PINC=MINC=1 ,
PSIZE=32-bit and MSIZE=16-Bit,
PINCOS=0
I saw somethings about packing and padding for stm32f4 DMA in RM0090,but I can't understand it.
Thanks.
2021-01-08 12:40 AM
Thanks.
I will test it.