2018-12-22 4:38 AM
Hi
I wish to use an external clock into PH0 from an oscillator module already present in my design.
Does this mean PH1 becomes a spare pin?
Thanks
Andy.
2018-12-22 5:00 AM
HSEBYP needs HSEON and HSEON withh use PH0/1. I fear you can't use PH1 with external HSE. Perhaps try do some experiments . Perhaps PH1 is usable as Input pin.
2018-12-22 5:02 AM
Hi Uwe
Will probably have to give it a try if I don't get a definite answer.
Thanks
Andy.
2018-12-23 4:03 AM
RM0090 clearly says:
The external clock signal (square, sinus or triangle) with ~50% duty cycle has to drive the OSC_IN pin while the OSC_OUT pin should be left HI-Z.
Also ch.8.3.14 Using the OSC_IN/OSC_OUT pins as GPIO PH0/PH1 port pins says that PH0/PH1's GPIO is overridden when HSEON is set.
But of course an experiment is worth thousand words.
JW
2020-12-17 8:43 AM
I have the same situation on a NucleoL053 where a 8MHz signal is supplied to the STM32L053 on the PH0 pin. The PH1_pin seems not to be controllable and stays Hi_Z.
2020-12-17 9:14 AM
STM32L072CZ PH1 not a GPIO w/BYPASS
Ran into this with the Grashopper LoRa board, see this thread for context
https://community.st.com/s/feed/0D50X00009bLS7uSAG
2020-12-17 9:41 AM