2015-10-16 2:31 AM
Good day,
I use CooCox 1.7.8 and STM32F4DISCOVERY as programmator. Problem is, that after re-configuring SysClk to PLL running on 168MHz (which is confirmed through observing 84MHz on MCO1 output) ToggleBit command produce no effect on LED's. If decrease SysClk to 42MHz, everything is working. Please see code below: ***#include ''stm32f4xx.h''
#include ''stm32f4xx_gpio.h'' </p>
</b>
#include ''stm32f4xx_rcc.h''
GPIO_InitTypeDef
GPIO_InitStruct;int i, k=0, l=0; </p>
</b>
int
main(
void
){
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE,
ENABLE
);GPIO_InitStruct.
GPIO_Pin
= GPIO_Pin_8|GPIO_Pin_10;
// we want to configure LED's: D1, D3
GPIO_InitStruct.
GPIO_Mode
=
GPIO_Mode_OUT
;
// we want it to be an OutputGPIO_InitStruct.
GPIO_Speed
=
GPIO_Speed_100MHz
;
//this sets the GPIO modules clock speedGPIO_InitStruct.
GPIO_OType
=
GPIO_OType_PP
;
// this sets the pin type to push / pull (as opposed to open drain)
GPIO_InitStruct.
GPIO_PuPd
=
GPIO_PuPd_NOPULL
;
// this disables the pull-down resistor GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_SetBits(GPIOE, GPIO_Pin_8|GPIO_Pin_10);
// LED1, LED3 On
for
(i=0; i<50000; i++);
//Wait
GPIO_ResetBits(GPIOE, GPIO_Pin_8|GPIO_Pin_10);
// LED1, LED3 Off/* Output HSE clock on MCO1 pin(PA8) ****************************************/
/* Enable the GPIOA peripheral */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,
ENABLE
);/* Configure MCO1 pin(PA8) in alternate function */
GPIO_InitStruct.
GPIO_Pin
= GPIO_Pin_8;GPIO_InitStruct.
GPIO_Speed
=
GPIO_Speed_100MHz
;GPIO_InitStruct.
GPIO_Mode
=
GPIO_Mode_AF
;GPIO_InitStruct.
GPIO_OType
=
GPIO_OType_PP
;GPIO_InitStruct.
GPIO_PuPd
=
GPIO_PuPd_UP
;GPIO_Init(GPIOA, &GPIO_InitStruct);
/* (PLL_clock/2) selected to output on MCO1 pin (PA8)*/
RCC_MCO1Config(RCC_MCO1Source_PLLCLK, RCC_MCO1Div_2);
RCC_PLLConfig(RCC_PLLSource_HSI, 0x08, 0xA8, 0x02, 0x07);
//PLLM=8 (2MHz), PLLN=168 (336MHz), PLLP=2 (SYS=168), PLLQ=7 (USB=48)
RCC_PLLCmd(
ENABLE
);
//Enable PLL using HSI
while
(!RCC_GetFlagStatus(RCC_FLAG_PLLRDY));
//Wait till PLL frequency established (23) RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
//Choose PLL as SYSCLK
for
(i=0; i<16800; i++);
//Wait
while
(1){
GPIO_ToggleBits(GPIOE, GPIO_Pin_8|GPIO_Pin_10);
// LED1, LED3 On
for
(i=0; i<1680; i++);
//Wait GPIO_ToggleBits(GPIOE, GPIO_Pin_8|GPIO_Pin_10);
// LED1, LED3 On
for
(i=0; i<1680; i++);
//Wait }***
As well, under debugger last while(1) reach its end successfully
(using breakpoints) but after it hangs.
Thanks in advance,
Konstantin
2015-10-16 3:01 AM
Observe the LED pin with oscilloscope.
JW2015-10-16 6:05 AM
2015-10-16 7:06 AM
Do you have the FLASH latency set properly?
JW2015-10-16 8:19 AM
As Jan indicates there is the flash wait state setting, but also where the AHB/APB clocks are set, and enable the High Performance Power mode.
CooCox has this broken interpretation of the CMSIS requirement to call SystemInit() to set up the clocks prior to setting the C Environment up and calling main()2015-10-19 3:50 AM
Thanks everyone.
FLASH->
ACR
|= FLASH_ACR_LATENCY_5WS;solves problem.!!.
BR. K.As Jan indicates there is the flash wait state setting, but also where the AHB/APB clocks are set, and enable the High Performance Power mode.
CooCox has this broken interpretation of the CMSIS requirement to call SystemInit() to set up the clocks prior to setting the C Environment up and calling main()We’re moving the ST Community to a new platform to give you a better and more reliable community experience.