cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 Dual DAC Independent Trigger Sources

yousef
Associate
Posted on September 27, 2016 at 08:54

Hello,

I have a problem for using both DACs of STM32F407 with independent trigger sources. 

What I did was directing DAC1 for Timer6 and DAC2 for Timer7 but they are still both triggered by one source (Timer6) and not independent as described. I set TSEL1 and TSEL2 for the sources accordingly (TIM6_TRGO, TIM7_TRGO). 

I tested both Timer Interrupts to be invoked as working.

DMA is not used in my case.

Are there any known issues for this topic?

Thanks in advance, Sebastian.
2 REPLIES 2
mark239955_stm1
Associate II
Posted on September 27, 2016 at 14:12

If you're not using DMA, why are you triggering the DAC's from timers?  What is it that you're trying to achieve?

Posted on September 27, 2016 at 17:49

Are there any known issues for this topic?

Haven't heard of any, and don't plan to independently verify. If you want someone to review the code for errors/issues, you'll want to post a sufficiently complete example.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..