cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407 Discovery RTC

vinothraj
Associate II
Posted on September 06, 2012 at 07:55

i try to show the time in Hiper terminal using uart.my problem  is moreover this link-

 

/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/stm32f4+dicovery++problems+coming+in+configuring+RTC.only+few+corrections+needed&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=154♯{2E8F2AEA-E1AC-4359-9FBC-341F279053F3}

       

the control flow is stuck on this place

while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET)

  {

  }

i think that i mistook on  

oscillating frequency.BUT could not find it.attached the files.you may refer it please.

#rtc #wait-for-you--clive1-!-!-!
20 REPLIES 20
Posted on January 28, 2014 at 21:12

I've had success with these EPSON MC-306 32.768K-E3:ROHS too.

http://www.mouser.com/search/ProductDetail.aspx?qs=tC2qD9afNgo5wsiSIyW37w%3D%3D

Note that some of the DISCOVERY boards also lack the 0 OHM resistors connecting the base of the crystal, but these are usually small enough to solder bridge. Most of the boards use 0402 caps, at least one uses 0603

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..