cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 and HC-05(bluetooth)

jota
Associate
Posted on September 28, 2015 at 19:00

Hello! First of all let me start by telling you that i'm a trully beginner.

So, im trying to receive a string like ''hello world'' in the termite .

I already can see the bluetooth hc-05 though my phone. I can connect the bluetooth on the termite however i cant receave anything from it.

My code is the following:

/* Includes ------------------------------------------------------------------*/

#include ''stm32f4_discovery.h''

#include ''stm32f4xx_gpio.h''

#include ''stm32f4xx_rcc.h''

#include ''stm32f4xx.h''

#include ''stm32f4xx_usart.h''

#include <string.h>

#include <stdio.h>

GPIO_InitTypeDef              GPIO_InitStructure;

USART_InitTypeDef             USART_InitStructure;

void delay(unsigned long tempo) {

                                                    volatile unsigned long i;

                                                    i = tempo;

                                                   do i-- ;

                                                   while (i !=0);

                                                  }

void USART_put(USART_TypeDef* USARTx, volatile char *s){

    while(*s){

        // wait until data register is empty

        while( !(USARTx->SR & 0x00000040) );

        USART_SendData(USARTx, *s);

        while(USART_GetFlagStatus(USART3, USART_FLAG_TC) == RESET)

                {

                }

        *s++;

    }

}

void GPIO_USART_Configuration(void){

     RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

     RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

     /* Configure USART Tx as alternate function  */

       GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

       GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

       GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

       GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

       GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

       GPIO_Init(GPIOC, &GPIO_InitStructure);

     /* Connect PXx to USARTx_Tx*/

       GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3);

 }

 void USART3_Configuration(void)

 {

         USART_InitStructure.USART_BaudRate = 38400;

         USART_InitStructure.USART_WordLength = USART_WordLength_8b;

         USART_InitStructure.USART_StopBits = USART_StopBits_1;

         USART_InitStructure.USART_Parity = USART_Parity_No;

         USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

         USART_InitStructure.USART_Mode = USART_Mode_Tx;

         USART_Init(USART3, &USART_InitStructure);

         USART_Cmd(USART3, ENABLE); // enable USART2

 }

void usart_inisialisasi()

 {

     GPIO_USART_Configuration();

     USART3_Configuration();

 }

int main(void) {

SystemInit();

usart_inisialisasi();

}

(obviously i tried to use usart_put but i cant use it correctly i think)

0690X00000602vLQAQ.jpg

any help would be appreciated.

Thank you,
2 REPLIES 2
Posted on September 28, 2015 at 19:32

So you're got something like

while(1)

USART_put(USART3, ''Hello World!\r\n'');

Right?

Have you configured the HC-05 to be at 38400 baud, at it's end not the phone's end? Or is this it's default?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jota
Associate
Posted on September 28, 2015 at 19:42

yes my code was something like that but i cant put it working. the baud-rate is correct . maybe something with the connections on the stm32 to the bluetooth? i only connected the bluetooth rx - stm usart3 tx ; bluetooth tx - stm usart3 rx ; vcc and ground. 

thanks for trying to help and replying me . really really aprecciated!