STM32F4 USB VCP problem with timeout when send data from PC to device
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-18 3:11 AM
Posted on January 18, 2015 at 12:11
Hello.
I am use example VCP from the ST. on STM32f405I am working under WinXP with a virtual COM port via the API as a file.Cyclically sends data (short packets from 8 to 16 bytes) from PC to Device by function - WriteFile.Data transfer immediately, but from time to time there is a strange TimeOut to transfer (WriteFile) sometimes up to 500ms.Same work, but with a real COM port, such delays are not present.What could be the problem?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0