2012-09-29 6:24 PM
I am using the following code to transfer an array of 100 elements to the PC via UART. I am not able to understand what my mistake is. Can someone please point out my mistake. Here is the code
USART_InitTypeDef USART_InitStructure;GPIO_InitTypeDef GPIO_InitStructure; /* Peripheral Clock Enable -------------------------------------------------*/ /* Enable GPIO clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC , ENABLE); /* Enable USART clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); /* Connect USART pins to AF7 */ GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3); /* Configure USART Tx and Rx as alternate function push-pull */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOC, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; /* When using Parity the word length must be configured to 9 bits */ USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Tx; USART_Init(USART3, &USART_InitStructure); USART_ClearFlag(USART3, USART_FLAG_TC); /* Enable USART */ USART_Cmd(USART3, ENABLE); SRAM_ReadBuffer(RxBuffer, 0x00, 100); for(i=0;i<100;i++) { USART_SendData(USART3, RxBuffer[i]); Delay(1000);*** while(USART_GetFlagStatus(USART3,USART_FLAG_TC) == RESET) {} USART_ClearFlag(USART3, USART_FLAG_TC); }The line marked as ***. I have tried it with both set and reset but to no avail.2012-09-30 5:43 AM
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Peripheral Clock Enable -------------------------------------------------*/
/* Enable GPIO clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC , ENABLE);
/* Enable USART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* Connect USART pins to AF7 */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_USART3);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_USART3);
/* Configure USART Tx and Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_Init(GPIOC, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
/* When using Parity the word length must be configured to 9 bits */
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;
USART_Init(USART3, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART3, ENABLE);
SRAM_ReadBuffer(RxBuffer, 0x00, 100);
for(i=0;i<100;i++)
{
while(USART_GetFlagStatus(USART3,USART_FLAG_TXE) == RESET);
USART_SendData(USART3, RxBuffer[i]);
}
2012-10-03 7:33 AM
Thanks a lot..works perfectly now...i really admire the way you have solved everyones problems in this forum..great...thanks again