cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 OSC Problem

Scarlet
Associate III

Hi everyone

I'm currently using the NUCLEO-F429ZI development board. I'm planning to create a PCB using the STM32F429ZIT6, but I've encountered some questions during the planning stage.

  1. According to the datasheet, HSE_OSC is specified to provide 8MHz, and CubeIDE also indicates "Input Freq HSE = 8MHz." However, on the NUCLEO-F429ZI development board, the JFVNY 25.000 oscillator supplies 25MHz. I have verified that the SPI clock indeed derives from multiplying and dividing an 8MHz source, but when I measure the JFVNY 25.000 oscillator on the development board, it does indeed supply 25MHz. Why are these two frequencies inconsistent, or am I misunderstanding something?
  2. Referring to the Clock tree and considering, if not using the RTC section, is it possible to omit providing the external LSE_OSE?
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20

I got it.

The crystal is used to active the MCU oscillator circuitry.

Normally, I called the crystal oscillator as the oscillator, so I overlooked the difference between the two.