2013-12-22 5:55 AM
Hello.
I'm using mp45dt02 mic on the discovery board and just forwarding data to cs43l22. For sampling freq 16k is working fine, but if I want higher Fs, it doesn't work anymore. I'm only hearing beeping/scratching from dac. Playing some 48k sound from flash works fine, so cs43l22 must be ok. I must be doing something wrong with the mic.I can provide cs43l22 code and/or hex files if someone will be interested.Here is the code for mp45dt02:&sharpinclude <stdint.h>&sharpinclude ''stm32f4xx.h''&sharpinclude ''stm32f4xx_rcc.h''&sharpinclude ''stm32f4xx_gpio.h''&sharpinclude ''stm32f4xx_spi.h''&sharpinclude ''pdm_filter.h''&sharpinclude ''queve.h''//sampling frequency&sharpdefine FS 16000//PDM decimation factor&sharpdefine DECIMATION 64//clock for mic&sharpdefine I2S_CLK ((FS*DECIMATION)/(16*2))//uint16_t array length for filter input buffer&sharpdefine MIC_IN_BUF_SIZE ((((FS/1000)*DECIMATION)/8)/2)//uint16_t array length for filter output buffer&sharpdefine MIC_OUT_BUF_SIZE (FS/1000)static PDMFilter_InitStruct pdm_filter;static uint16_t mic_in_buf[MIC_IN_BUF_SIZE];static uint16_t mic_out_buf[MIC_OUT_BUF_SIZE];static uint32_t mic_buf_index;void mp45dt02_init(){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE); pdm_filter.LP_HZ=8000; pdm_filter.HP_HZ=10; pdm_filter.Fs=FS; pdm_filter.Out_MicChannels=1; pdm_filter.In_MicChannels=1; PDM_Filter_Init(&pdm_filter); //MP45DT02 CLK-PB10 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitTypeDef gpio; gpio.GPIO_Pin=GPIO_Pin_10; gpio.GPIO_Mode=GPIO_Mode_AF; gpio.GPIO_OType=GPIO_OType_PP; gpio.GPIO_PuPd=GPIO_PuPd_NOPULL; gpio.GPIO_Speed=GPIO_Speed_50MHz; GPIO_Init(GPIOB, &gpio); GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_SPI2); //MP45DT02 DOUT-PC3 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); gpio.GPIO_Pin=GPIO_Pin_3; gpio.GPIO_Mode=GPIO_Mode_AF; gpio.GPIO_OType=GPIO_OType_PP; gpio.GPIO_PuPd=GPIO_PuPd_NOPULL; gpio.GPIO_Speed=GPIO_Speed_50MHz; GPIO_Init(GPIOC, &gpio); GPIO_PinAFConfig(GPIOC, GPIO_PinSource3, GPIO_AF_SPI2); NVIC_InitTypeDef nvic; nvic.NVIC_IRQChannel = SPI2_IRQn; nvic.NVIC_IRQChannelPreemptionPriority = 1; nvic.NVIC_IRQChannelSubPriority = 0; nvic.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&nvic); //I2S2 config RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); RCC_PLLI2SCmd(ENABLE); while(!RCC_GetFlagStatus(RCC_FLAG_PLLI2SRDY)); I2S_InitTypeDef i2s; i2s.I2S_AudioFreq=I2S_CLK; i2s.I2S_Standard=I2S_Standard_LSB; i2s.I2S_DataFormat=I2S_DataFormat_16b; i2s.I2S_CPOL=I2S_CPOL_High; i2s.I2S_Mode=I2S_Mode_MasterRx; i2s.I2S_MCLKOutput=I2S_MCLKOutput_Disable; I2S_Init(SPI2, &i2s); I2S_Cmd(SPI2, ENABLE);}void mp45dt02_start(){ SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_RXNE, ENABLE);}void SPI2_IRQHandler(){ if(SPI_GetITStatus(SPI2, SPI_I2S_IT_RXNE)){ uint16_t sample=SPI_I2S_ReceiveData(SPI2); mic_in_buf[mic_buf_index++]=HTONS(sample); if(mic_buf_index == MIC_IN_BUF_SIZE){ mic_buf_index=0; PDM_Filter_64_LSB((uint8_t *)mic_in_buf, mic_out_buf, 40, &pdm_filter); uint32_t i; for(i=0; i<MIC_OUT_BUF_SIZE; i++){ enqueve(mic_out_buf[i]); } } }}Thanks. #stm32f4discovery-mp45dt022014-12-31 6:27 AM
Is my input and output buffer length correct?
I attached compiled program which in infinite loop firstly recording for 1 sec and then playing recorded sound. You can hear scratching. I also noticed that at record cycle dac sometimes outputs noise and sometimes nothing. Compiler is gcc arm embedded 4.7 and I compiled with -Os ________________ Attachments : mic_48k.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzni&d=%2Fa%2F0X0000000bPp%2FrSYLRaQGY.S63RWld382S_Z5wKJ7rWWqCyleV_vb97Y&asPdf=false2016-08-15 11:34 PM
hey, i am working on the same project. Trying to capture audio and playing it back. I am facing a lot of issues trying to get it work. Can you please mail me the complete project with all the header and source files so that i can get a better understanding about it?
I would be highly obliged.email-id : jainpl15.extc@coep.ac.in