STM32F4 I2C BTF bit is not set after DMA TX complete
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-12-10 9:29 AM
Posted on December 10, 2012 at 18:29
Hi all,
I noticed that there is an high traffic in I2C2_EV_IRQHandler() with status 0x70080 (EV8 =I2C_EVENT_MASTER_BYTE_TRANSMITTING) after all the bytes was transmitted with success by DMA (but it's the same problem without DMA transfer).I think the reason is that the TXE is still set, and the BTF is not (hardware will set it after several 0x70080 interrupts).So, is there a way to force BTF to 1 after DMA IT TC ? Is it a DMA control register parameter to set ?Even after that (BTF is set now), I noticed several interrupts with same status (0x70084 = EV8_2 = I2C_EVENT_MASTER_BYTE_TRANSMITTED), all of this repeated interrupts are useless for me.Of course, it's not a problem for a simple TX write operation, because I can disable interrupts after sending the stop condition, but when I want to restart for a RX read sequence, it's alot of interrupts that are fired for nothing.I think there may be a way to fix it ? don't it ? #i2c-stm32f4-dma
Labels:
- Labels:
-
I2C
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-12-12 5:45 AM
Posted on December 12, 2012 at 14:45
Hi Stephane,
In the I2C_ITConfig, don't enable the buffer interrupt (I2C_IT_BUF). If this is already the case, please share the DMA and I2C config for a deeper investigation. Cheers, STOne-32Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-12-13 4:51 AM
Posted on December 13, 2012 at 13:51
Hi STOne-32,
And tx for your answer.In fact I'm re-writing my DMA+INT configuration by reading carefully the datasheet, and I'm a bit confused about initialization sequence, cause it appears I was doing wrong sequence before (strange random freeze, strange status, and I2C_IT_BUF was enable, you were true...).So could you please tell me if I'm wrong somewhere with the new configuration.- first init of the dma_channels (with DMA_Cmd( DMAx_Streamx, ENABLE ), and I2C_DMACmd(I2Cx, DISABLE))- Then, TX I2C transaction begin with I2C_ITConfig(I2Cx, I2C_IT_BUF, DISABLE);START -> 30001 : send_addr() -> 70082 : and if everything is ok, DMA transfer should begin automaticaly when 70080 ?But when should I set : I2C_DMACmd(I2C2, ENABLE) ?I tried at 30001 and after 70082, but I don't catch a DMA_IT_TCIFx interrupt...I tried with or without clock stretching, other configs, but DMA is never ended ??