2012-04-21 11:16 PM
I have configured my time 1 to operate in the PWM mode1 to generate a signal of fixed duty cycle. I want the generate an update INT every 4 th overflow of the TIM1 CNT . I have loaded value 4 into my repetition counter, which should decrement each time the CNT in TIM1 overflows and should generate an update INT when it reaches 0. I compute the duty cycle in the ISR and load it onto the preload registers.
The registers which i configure for the timer to operate in the above mentioned mode are given below: TIM1 CR1 URS -> 1 // update request source TIM1 RCR RCR -> 4 // loads 4 into the reconfiguration register TIM1 DIER UIE -> 1 // update interrupt enable A snippet of the code when in i initialize the registers is posted below: int main(void) { /* TIM Configuration */ TIM_Config(); /* Compute the prescaler value */ PrescalerValue = (uint16_t) ((SystemCoreClock /2) / 28000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter=4; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Configures the TIMx Prescaler. */ TIM_PrescalerConfig(TIM1,PrescalerValue,TIM_PSCReloadMode_Update); /* PWM1 Mode configuration: Channel3 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable); /* Configures the TIM1 Update Request Interrupt source (SETS the CR1->URS bit)*/ TIM_UpdateRequestConfig(TIM1,TIM_UpdateSource_Regular); /*Enables or disables TIM1 peripheral Preload register on ARR */ TIM_ARRPreloadConfig(TIM1, ENABLE); /* TIM1 enable counter */ TIM_Cmd(TIM1, ENABLE); /*Enables or disables the TIM peripheral Main Outputs*/ TIM_CtrlPWMOutputs(TIM1, ENABLE); /* Enables or disables the specified TIM interrupts */ TIM_ITConfig(TIM1,TIM_IT_Update, ENABLE); while (1) {} } If correct me if i have missed any steps in configuring TIM1 to generate an update interrupt every 4th overflow of the CNT ( which is achieved using the Repetition counter). -Regards -Gandalf2012-04-22 7:34 AM
It doesn't look unreasonable, no idea if you're initializing the clock source or the NVIC suitably.
Have you tested it? Is some aspect not working?2012-04-22 10:58 PM
Thanks for the heads up. I forgot the initialize the NVIC.
-Gandalf