2014-11-04 3:34 AM
2014-11-04 6:58 AM
Hi all,
problem solved. Had issues with the Button_Init and Uart_Init. Now the only problem left is, the screen is mirrored and the colors dont match yet ...2014-11-04 7:10 AM
Now the only problem left is, the screen is mirrored and the colors dont match yet ...
The only hint I can give is to read the SSD1963 specification carefully (especially the configuration register part), and compare it with your actual screen initialisation. It shouldn't be too difficult to find the init values for screen orientation and colour modes. I have done the same (only for other screen controllers). Sometimes (say, often) subvariants differ here on small details. BTW, there is a ''Format Code Block'' icon available when editing your post (upper left icon), which makes code snippets much more readable ...2014-11-04 12:29 PM
Hi fm,
thanks for your answer! I will try to figure out the init problem tomorrow. Thanks for the hint with the Format Code Button ;)2014-11-05 2:41 AM
Hi again,
i got the mirrored screen working in the correct way, but i still have color and performance problems. Also i can't figure out how to display an image correctly. The image is converted with the tool vader.darth used in his old project, but i can only see half of the image on the screen. Here is my SSD1963 LCD_init:
/*******************************************************************************
* Function Name : LCD_Initializtion
* Description : SSD1963 Resets
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void LCD_Init(void)
{
// Reset
GPIO_ResetBits(GPIOB , GPIO_Pin_0);
Delay_ms(300); //changed 300 to 30 2014
GPIO_SetBits(GPIOB , GPIO_Pin_0);
Delay_ms(300); //changed 300 to 10 2014
LCD_WriteIndex(SSD1963_SOFT_RESET); //Software Reset
LCD_WriteIndex(SSD1963_SOFT_RESET); //Software Reset
LCD_WriteIndex(SSD1963_SOFT_RESET); //Software Reset
Delay_ms(500);
//Set_PLL
LCD_WriteIndex(SSD1963_SET_PLL); //START PLL changed from WriteReg to index
LCD_WriteData(0x01); //added 2014
Delay_ms(1000); //required delay
LCD_WriteData(0x03); //LOCK PLL
Delay_ms(5);
LCD_WriteIndex(SSD1963_SOFT_RESET); //Soft replacement
Delay_ms(20);
// Back Light
GPIO_SetBits(GPIOC , GPIO_Pin_7);
Delay_ms(10);
//Set LCD mode, varies from individual manufacturer
LCD_WriteIndex(SSD1963_SET_GDISP_MODE);
LCD_WriteData(0x20); // set 24-bit for AT070TN92 7'' panel
LCD_WriteData(0x00); // set Hsync+Vsync mode changed 0x00 to 0x20 2014
LCD_WriteData((DISP_HOR_RESOLUTION-1)>>8); // Set LCD panel size(DISP_HOR_RESOLUTION = 800) H Changed 480 to 800 2014
LCD_WriteData(DISP_HOR_RESOLUTION-1); // Set LCD panel size(DISP_HOR_RESOLUTION = 800) L Changed 480 to 800 2014
LCD_WriteData((DISP_VER_RESOLUTION-1)>>8); // Set LCD panel size(DISP_VER_RESOLUTION = 480) H Changed 272 to 480 2014
LCD_WriteData(DISP_VER_RESOLUTION-1); // Set LCD panel size(DISP_VER_RESOLUTION = 480) L Changed 272 to 480 2014
LCD_WriteData(0x00); //0x00 // RGB sequence
Delay_ms(5);
/* added 2014
* For a 10MHz reference clock to obtain 115MHz PLL frequency, user cannot program N = 23 and M = 2. The closet
setting in this situation is setting N=34 and M=3, where 10 x 34 / 3 = 33MHz.
WRITE COMMAND “0xE2�?
WRITE DATA “0x21�? (N=34)
WRITE DATA “0x02�? (M=3)
WRITE DATA “0x54�? (Dummy Byte)
*/
LCD_WriteIndex(SSD1963_SET_PLL_MN); //Set PLL with OSC = 10MHz (hardware), Multiplier N = 35,
//250MHz <
VCO
<
800MHz
=
OSC
*(N+1),
VCO
=
360MHz
LCD_WriteData(0x22); //
OSC
=
10MHz
(hardware),// Parameter 1 changed from 0x23 to 0x22 2014
LCD_WriteData(0x02); //Parameter 2 Divider
M
=
2
,
PLL
=
360
/(M+1) = 120MHz
LCD_WriteData(0x54); //Parameter 3 Validate M and N values
Delay_ms(5);
// LCD_WriteIndex(0xE6); // SET PCLK
freq
=
6
.5MHz/19MHz, pixel clk freq added2014
// LCD_WriteData(0x00);
// LCD_WriteData(0xEA);
// LCD_WriteData(0xEC);
//Set horizontal period
LCD_WriteIndex(SSD1963_SET_HORI_PERIOD);
LCD_WriteData((LCD_HT-1)>>8); //Set HT
LCD_WriteData(LCD_HT-1);
LCD_WriteData((LCD_HPS-1)>>8); //Set HPS
LCD_WriteData(LCD_HPS-1);
LCD_WriteData(DISP_HOR_PULSE_WIDTH-1); //Set HPW
LCD_WriteData(0x00);
LCD_WriteData(0x00);
LCD_WriteData(0x00);
Delay_ms(5);
//Set vertical period
LCD_WriteIndex(SSD1963_SET_VERT_PERIOD);
LCD_WriteData((LCD_VT-1)>>8); //Set VT
LCD_WriteData(LCD_VT-1);
LCD_WriteData((LCD_VPS-1)>>8); //Set VPS
LCD_WriteData(LCD_VPS-1);
LCD_WriteData(DISP_VER_PULSE_WIDTH-1); //Set VPW
LCD_WriteData(0x00); //Set FPS
LCD_WriteData(0x00);
Delay_ms(5);
//Set LSHIFT freq, i.e. the DCLK with PLL freq 120MHz set previously
//To obtain PCLK = 5.3MHz with PLL Frequency = 120MHz,
//5.3MHz = 120MHz * LCDC_FPR / 2^20
//LCDC_FPR = 46312
LCD_WriteIndex(SSD1963_SET_LSHIFT_FREQ);
LCD_WriteData(0x00); //changed from 0x01 to 0x00 according to Display Datasheet 2014
LCD_WriteData(0xB4); //changed from 0x33 to 0xB4 according to Display Datasheet 2014
LCD_WriteData(0xE7); //changed from 0x32 to 0xE7 according to Display Datasheet 2014
Delay_ms(5);
LCD_WriteIndex(SSD1963_SET_PIXEL_FORMAT); //Set pixel format, i.e. the bpp
LCD_WriteData(0x50); // set 16bpp --> 101
Delay_ms(5);
LCD_WriteIndex(SSD1963_SET_PIXEL_DATA_INTERFACE); // Set pixel data interface
LCD_WriteData(SSD1963_PDI_16BIT565); //16-bit(565 format) data for 16bpp
Delay_ms(5);
LCD_WriteIndex(SSD1963_ENTER_NORMAL_MODE); // SET normal mode added 2014
LCD_WriteIndex(SSD1963_SET_ADDRESS_MODE); //added 2014
LCD_WriteData(0x02); //changed from 2 to 0x02 2014 correct orientation
//see SSD1936 datasheet figure 9-12 to 9-15
LCD_WriteIndex(SSD1963_EXIT_INVERT_MODE); //added 2014
LCD_WriteIndex(SSD1963_SET_COLUMN_ADDRESS); // Set column address added 2014
LCD_WriteData(0x00); //SET start column address=0
LCD_WriteData(0x00);
LCD_WriteData(0x03); //SET end column address=800
LCD_WriteData(0x1F);
LCD_WriteIndex(SSD1963_SET_PAGE_ADDRESS); //SET page address added 2014
LCD_WriteData(0x00); //SET start page address=0
LCD_WriteData(0x00);
LCD_WriteData(0x01); //SET end page address=480
LCD_WriteData(0xDF);
LCD_WriteIndex(SSD1963_SET_SCROLL_AREA); //SET scroll area added 2014
LCD_WriteData(0x00);
LCD_WriteData(0x00);
LCD_WriteData((DISP_VER_RESOLUTION)>>8); //Set VerticalScrollArea
LCD_WriteData(DISP_VER_RESOLUTION);
LCD_WriteData(0x00);
LCD_WriteData(0x00);
LCD_WriteIndex(SSD1963_SET_SCROLL_START); //SET scroll start added 2014
LCD_WriteData(0x00); //Set VerticalScrollPointer
LCD_WriteData(0x00);
LCD_WriteIndex(SSD1963_EXIT_IDLE_MODE); //full color depth added 2014
LCD_WriteIndex(SSD1963_SET_DISPLAY_ON); // Turn on display
LCD_WriteIndex(SSD1963_WRITE_MEMORY_CONTINUE); //added 2014
//Delay_ms(5);
}
Maybe somebody can see where the problem is causing the color malfunction. I attached the Display datasheet and the SSD1963 manual.
________________
Attachments : AT070TN92_V.1-Datasheet.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzdK&d=%2Fa%2F0X0000000bQ2%2FuNd2XINSfsAK8F8jEnneUkjNY78_VMCC8iT9PNKRjqI&asPdf=falseSSD1963.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzp5&d=%2Fa%2F0X0000000bQ3%2FKABI3u1PLs80StLjr5IVC3DmBvAtyCxRZSTHd7MsrLU&asPdf=false