2012-07-23 10:53 AM
I got 2 new STM32F4 Discovery boards and both are not being recognized by STLINK utility. Here some of the observations. I compared the behavior to STM32F1 discovery board. (It is Windows 7 PC).
1) Plug in STM32F1 board. I see a pop up window saying USB mass storage device found.Plug in STM32F4. No window pops up.2) In STLink Utility I press the connect button. STM32F1 board is found and I can download program to flash. With STM32F4 I get a error message saying ''No STlink device found''My board has Rev Z devices. I tried the patch that was released to support Rev Z device. That did not work either.If we forget about programming the target device, I am not sure if the basic USB connection to the STLink is working. Any way to test/confirm this.Thanks #stm32f4discovery-stm32f42012-07-23 12:07 PM
Do any of the LEDs illuminate? The STM32F4 has two USB connectors, only the Micro-B connects to ST-LINK and supplies power to the board.
2012-07-23 12:17 PM
Yes, I have used the Micor-B connector. The LED's are lit up and 4 leds surrounding the accelerometer are blinking. The default accelerometer program is working and changes the LEDS as I tilt the board.
If I disconnect the target from the STLink by opening the jumpers, there is no change. The STLink is still not found.2012-07-23 12:33 PM
Go to Device Manager and confirm it's found the USB Device
Universal Serial Bus Controllers STMicroelectronics STLink Dongle C:\Windows\system32\DRIVERS\WinUSB.sys 6.1.7601.17514 (win7sp1_rtm.101119-1850) Keil shows it as ST-Link deprecated. This is on a Win7 x64 system. Check you have suitable drivers installed.2012-07-23 2:06 PM
I think I got it working. Had to uninstall everything and re-install. Plus I think earlier I had STLink driver as opposed to STLink V2 driver.
Even with STLink V2 driver installed, the device manager was showing as unrecognized and had yellow icon showing driver issues. I had to chose the device and update driver in device mananger. It worked after that. I will have to check to see if Rev. Z issue will show up when I try to program the target.2012-07-23 5:17 PM
Micro? I don't think so. Mini USB is for supply & ST-Link, Micro USB for USB OTG & stuff.
2012-07-24 4:13 AM
Micro? I don't think so. Mini USB is for supply & ST-Link, Micro USB for USB OTG & stuff.
Sorry, you're right the Mini-B, not the Micro-AB2012-09-24 1:44 PM
I've run into the same problem. ''USB device not recognized'' when I connect STM32F4 (rev. Z) board to my comp (Win 7, 64-bit). I have installed ST-LINK V2 USB driver. I tried to reinstall it but it didn't help. Please, can someone give me some advice what to try?
Thanks2012-09-25 1:08 PM
Try it on a different PC.
Check that Win7 is set to accept unsigned drivers.2012-09-29 1:57 PM
Hey all. I had the same problem. Version ''Z'', not being recognized at all by stlink utility or coocox coIDE while my stm32vl worked fine. Tried a bunch of fancy stuff, thought maybe it was dead on arrival..
I ended up just going into device manager and clicking on ''update driver'' and selecting the automatic search option. Windows7, 64bit. I know it's really dumb, but this extremely simple solution is what worked for me. Now it downloads and debugs (using coocox coIDE with armgcc) reliably. Hope that helps somebody.