cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4 discovery LIS3DSH HAL problem

borisbritwa13
Associate III
Posted on February 16, 2016 at 14:14

No answer from the register who I am.

The most interesting is that this code worked for a while, but now does not work.

I have

attached a file

that previously

all worked.

/* USER CODE BEGIN 0 */

uint8_t SPI_read(uint8_t address)

{

    uint8_t  reciveData;

    address = 0x80 | address;  

  CS_ON

    HAL_SPI_TransmitReceive(&hspi1,&address,&reciveData,1,100);

    uint8_t data=0x00;

    HAL_SPI_TransmitReceive(&hspi1,&data,&reciveData,1,100);

  CS_OFF

    return reciveData;

}

 /* USER CODE END 0 */

/* USER CODE BEGIN 2 */

RED_LED_ON

GREEN_LED_ON

if (SPI_read(0x0F)==0x3B){

    RED_LED_OFF

    }else if(SPI_read(0x0F)==0x3F)//LIS3DSH

    GREEN_LED_OFF

 /* USER CODE END 2 */

/* SPI1 init function */

void MX_SPI1_Init(void)

{

  hspi1.Instance = SPI1;

  hspi1.Init.Mode = SPI_MODE_MASTER;

  hspi1.Init.Direction = SPI_DIRECTION_2LINES;

  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;

  hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

  hspi1.Init.NSS = SPI_NSS_SOFT;

  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;

  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi1.Init.TIMode = SPI_TIMODE_DISABLED;

  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

  hspi1.Init.CRCPolynomial = 10;

  HAL_SPI_Init(&hspi1);

}    
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on February 18, 2016 at 07:50

Hi britwa.boris,

Could you please precise the updates you made so that we can deduce the cause of the problem you are facing? You said that previously it was working as expected.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

borisbritwa13
Associate III
Posted on February 20, 2016 at 13:35

Thanks for the reply

!!!

I wrote some

code

at the top of

that

I have used.

Sensor

replied

0x3F

(see

attached file

).

Then

I turned off

the board and

turned on

later

and the answer

of who I am

-

0xff

.I

noticed

early

that the code

at the top

does not work

if

I disable

the logic analyzer

(

I do not know

why it

happened

)

.

Now the code

is not working

,

so I

did

.

Now,

if you connect a

logic analyzer

and ask

SPI_read (0x0F)

all

look the same

but

in response

I see

0xFF

.

See

has attached

file!!!!

I

think it is not necessary

any

initialization

before you read

the register

who I am

?

I am very

upset .

Initially,

perhaps

in my actions

there is an error

.

I will be glad

to your opinion .

Had to dig

in smartphones

and

unsolder

the accelerometer

another brand

(

bma150

)

Under him have to make a Board

,

because

it is very small

.

________________

Attachments :

NOT_OK.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0ml&d=%2Fa%2F0X0000000bdd%2F3jwxa8ON69dV8nN3pyhXNoGV3roeleIMKSWKH1I4IJM&asPdf=false

Sam_file.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0mg&d=%2Fa%2F0X0000000bdb%2FuIUh19Wa2UjtpvuInQ778mTJTyycibMF9t2x09DuIHE&asPdf=false