Uart Rx interrupt not working if clock for GPIOD is enabled
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-02-20 6:31 AM
Posted on February 20, 2016 at 15:31
Hello.
I am using a custom board with STM32F030R8 as my dev platform. I am using Uart2 to configure the board. The RX interrupt is enabled to receive data. i am using PD2 as a GPIO.When i enable peripheral clock to GPIOD, i am not getting uart rx interrupt but uart tx works fine. But when i do not enable the GPIOD peripheral clock everything works fine.I have no idea what is the problem here...Is there something i am missing here?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0