2014-11-09 3:19 PM
Hi!
I have stm32f4 discovery board MB997C.
I`m trying to communicate with LIS3DSH accelerometer. I have a problem - MISO line (port PA6) is always high. I`m just trying to get the value of WHO_AM_I register and as response I always get 0xFF. Here is my configuration code: #define CS_HIGH GPIO_SetBits(GPIOE, GPIO_Pin_3) #define CS_LOW GPIO_ResetBits(GPIOE, GPIO_Pin_3)GPIO_InitTypeDef GPIOA_InitStructure;
GPIO_InitTypeDef GPIOE_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; SPI_InitTypeDef SPI_InitStructure;uint8_t receivedByte;
unsigned int TransactionFlag = 0x0000; unsigned int TransmitCounter = 0x0000;void main(void)
{ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); GPIOA_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; GPIOA_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIOA_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOA_InitStructure.GPIO_OType = GPIO_OType_PP; GPIOA_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIOA_InitStructure); GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource6,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource7,GPIO_AF_SPI1); GPIOE_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIOE_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIOE_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOE_InitStructure.GPIO_OType = GPIO_OType_PP; GPIOE_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOE, &GPIOE_InitStructure); CS_HIGH; SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_Init(SPI1, &SPI_InitStructure); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); SPI_Cmd(SPI1, ENABLE); // SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE); // SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_TXE, ENABLE); while(1) { unsigned long i;CS_LOW;
for(i = 0; i < 10; i++); SPI_I2S_SendData(SPI1, 0x8F); //Wait for transmission to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for received data to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); //Wait for SPI to be ready // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY)); receivedByte = SPI_I2S_ReceiveData(SPI1); SPI_I2S_SendData(SPI1, 0x00); //Wait for transmission to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for received data to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); receivedByte = SPI_I2S_ReceiveData(SPI1); //Wait for transmission to complete // while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for SPI to be ready // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY)); for(i = 0; i < 10; i++); CS_HIGH;for(i = 0; i < 100; i++);
} }Help me please, what am i doing wrong?