2016-09-10 11:32 AM
Hi everybody,
I'm writing this post to ask if someone, please, can help me resolving a problem with the datas-reading from the accelerometer integrated in the STM32F4 Evaluation Board.What I want to do it's simply to read the accelerations datas from the sensor, using the SPI interface. I've had a look at a lot of examples but I still don't know why my code doesn't work.Here the main functions:void WriteAccelerometer(SPI_HandleTypeDef SPI, uint8_t address, uint8_t data){ HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET); //CS --> Low HAL_SPI_Transmit(&SPI,&address,1,50); HAL_SPI_Transmit(&SPI,&data,1,50); HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET); //CS --> High} uint8_t ReadAccelerometer(SPI_HandleTypeDef SPI, uint8_t address, uint8_t data){ address = address | 0x80; HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET); //CS --> Low HAL_SPI_Transmit(&SPI,&address,1,50); HAL_SPI_Receive(&SPI,&data,1,50); HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET); //CS --> High return data;}Here the SPI configuration function:static void MX_SPI1_Init(void){ hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi1) != HAL_OK) { Error_Handler(); } //WriteAccelerometer(hspi1,0x23,0xC9); //reset //WriteAccelerometer(hspi1,0x21,0x00);}I use the two functions reported in this post to configurate and read the accelerometer with this commands:uint8_t config_address = 0x20;uint8_t config_data = 0x27; uint8_t Address_ACCX = 0x29;uint8_t Address_ACCY = 0x2B;uint8_t Address_ACCZ = 0x2D;WriteAccelerometer(hspi1,config_address,config_data); //config// read data:AccX = ReadAccelerometer(hspi1,Address_ACCX,AccX);AccY = ReadAccelerometer(hspi1,Address_ACCY,AccY);AccZ = ReadAccelerometer(hspi1,Address_ACCZ,AccZ);Thank you in advance for the help..Simone2017-10-31 4:42 AM
Yep, set ADDR 0x20 to 0x67 to initialise the MEMS and it responds to WHO_AM_I. Sometimes the temperature doesn't respond, but I found that on startup I reboot the MEMS by setting the BOOT bit high in 0x24 register.
My next problem is that my axes accelerations are static. I get a reading but it doesnt change at all. Any ideas?EDIT: i have posted my (simplified) code in another comment
2017-10-31 4:46 AM
My function definitions are:
void
MEMS_write(uint8_t
addr,uint8_t
data){
uint8_t
send[2] = {addr, data};HAL_GPIO_WritePin(
CS_I2C_SPI_GPIO_Port
, CS_I2C_SPI_Pin, LOW);HAL_SPI_Transmit(&hspi1, send, 2, 5000);
HAL_GPIO_WritePin(CS_I2C_SPI_GPIO_Port, CS_I2C_SPI_Pin, HIGH);
return
;
}
uint8_t
MEMS_read(uint8_t
addr){
uint8_t
send[1] = {0x80 | addr};
uint8_t
out[1] = {0x00};HAL_GPIO_WritePin(CS_I2C_SPI_GPIO_Port, CS_I2C_SPI_Pin, LOW);
HAL_SPI_TransmitReceive(&hspi1, send, out, 2, 0xFF);
HAL_GPIO_WritePin(CS_I2C_SPI_GPIO_Port, CS_I2C_SPI_Pin, HIGH);
return
out[1];}
My simplified main is: (omitting non-spi code for readability)
int main(void){
MEMS_write(0x24, 0b1000000);
//rebooting themems
seems to unlock it?HAL_Delay(100);
MEMS_write(0x20, 0x67); //enable x, y, z axes and ODR
MEMS_write(0x24, 0x01);
//3 wire
spi
while
(1){
MEMS_read(0x0F); //request WHO_AM_I
HAL_Delay(10);
}
}
2017-10-31 5:39 AM
Actually I tried to use the
LIS3DSH but no getting value.Maybe interested cpol and cpha now I have come home,I will look it and try.
2017-10-31 5:57 AM
Again no value ,Ok I am sending some code maybe you can understand my mistake.
if(HAL_SPI_GetState(hspi) == HAL_SPI_STATE_READY )
{ a = BW_RATE; b = 0x0D;HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(hspi,&a,1,100);//800Hz ODR , Normal mode HAL_SPI_Transmit(hspi,&b,1,100); HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_SET); a = POWER_CTL; b = 0x08; HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(hspi,&a,1,100);////Measurement mode HAL_SPI_Transmit(hspi,&b,1,100); HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_SET); } elseabove codes are to set.below codes are to get valuesdo
{ adress = INT_SOURCE | 0x80; HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(hspi,&adress,1,100); HAL_SPI_Receive(hspi,&temp,1,100); HAL_GPIO_WritePin(ADXL345_CS_GPIO_Port,ADXL345_CS_Pin, GPIO_PIN_SET);}while((temp & 0x80) == 0);
moving is stucking in loop.Am I wrong in this step '
adress = INT_SOURCE | 0x80; '
As much as I know this is a way to get value with SPI related 0x80.
2017-10-31 6:12 AM
Ahh you're not using the same MEMS as me. I'm using the LIS3DSH. Google SPI modes, and have a look what mode matches your ADXL datasheet and set your CPOL and CPHA accordingly.
Also as you are using a different ic, you will probably have different register addresses.
2017-10-31 2:13 PM
#define DATA_FORMAT (uint8_t)0x31
#define BW_RATE (uint8_t)0x2C#define POWER_CTL (uint8_t)0x2D#define FIFO_CTL (uint8_t)0x38#define DATAXL (uint8_t)0x32#define DATAXH (uint8_t)0x33#define DATAYL (uint8_t)0x34#define DATAYH (uint8_t)0x35#define DATAZL (uint8_t)0x36#define DATAZH (uint8_t)0x37#define OFSX (uint8_t)0x1E#define OFSY (uint8_t)0x1F#define OFSZ (uint8_t)0x20#define INT_ENABLE (uint8_t)0x2E #define INT_SOURCE (uint8_t)0x302017-10-31 2:15 PM
2017-10-31 2:18 PM
I am using STM32f4 discovery board,actually .SPI is working I controlled with Osciloscope also NRF24L01 is working and I2C is working same ADXL345 I mean device is strong.Also my new codes are here.
void ADXL345_Setup(SPI_HandleTypeDef *hspi)
{ if(HAL_SPI_GetState(hspi) == HAL_SPI_STATE_READY ) { ADXL345_Write_Single(hspi,BW_RATE,0x0D);ADXL345_Write_Single(hspi,POWER_CTL,0x08);
//ADXL345_Write_Single(hspi,DATA_FORMAT,0x04); } else { while(1) {}
}}//##################################################################################void ADXL345_Raw_Values(SPI_HandleTypeDef *hspi,int16_t *AccRaw){ uint8_t out[6]={0},temp=0;do
{ temp = ADXL345_Read_Single(hspi,INT_SOURCE); }while((temp & 0x80) == 0); ADXL345_Read_Multi(hspi,DATAXL,out,6);AccRaw[x_eksen] = (int16_t)(((uint16_t)out[1]<<8) | out[0]);
AccRaw[y_eksen] = (int16_t)(((uint16_t)out[3]<<8) | out[2]); AccRaw[z_eksen] = (int16_t)(((uint16_t)out[5]<<8) | out[4]);}//##################################################################################void ADXL345_Write_Single(SPI_HandleTypeDef *hspi, uint8_t reg, uint8_t data){ CS_LOW; HAL_SPI_Transmit(hspi,®,1,100); HAL_SPI_Transmit(hspi,&data,1,100); CS_HIGH;}//##################################################################################//##################################################################################uint8_t ADXL345_Read_Single(SPI_HandleTypeDef *hspi, uint8_t reg){ reg |= 0x80; // Okuma biti etkin // uint8_t out; CS_LOW; HAL_SPI_Transmit(hspi,®,1,100); HAL_SPI_Receive(hspi,&out,1,100); //HAL_SPI_TransmitReceive(hspi, &adr, &out, 1, 200); CS_HIGH; return out;}//##################################################################################//##################################################################################void ADXL345_Read_Multi(SPI_HandleTypeDef *hspi, uint8_t reg,uint8_t *out, uint8_t NumberOfByte){ reg |= 0xC0; // Okuma ve çoklu okuma bitleri etkin.0b1100-0000 // CS_LOW; HAL_SPI_TransmitReceive(hspi,®,out,NumberOfByte,100); CS_HIGH;}//##################################################################################//##################################################################################2017-10-31 2:19 PM
I am trying 2 days this.
2017-10-31 2:44 PM
I didnt manage to understand rhat you mean,sorry my late reply