cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f4-disco USART3 st link baudrate switch problem

SBolt.1
Associate

Dear Sirs or Madames,

I have a stm32f4-disco board with an adafruit winc1500 wifi shield. The firmware update and the update of the ssl certificates for the winc1500 are carried out via a serial bridge. While updating I have to switch a few times USART baudrate from 115200 to 500000 and vice versa. If I do this on USART3 stlink debug interface sometimes sent packages were lost. If I use USART6 which is without stlink debug interface everything works fine. Do you have any idea what could be the problem? Thanks in advance.

Best regards

Sebastian

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0