2015-07-20 12:54 PM
Hi there , I had my STM32F407VG discovery board for a while now, till a few minutes earlier, I was trying to interface a button to PA13 ( I chose PA13 randomaly) to create a simple interaface for my project , but once I tired the button few times I did not work, What's even worse now my Discovery board is not detected by CooCox and on the ST Link Utility it says ''Cannot Connect to target , please Connect under Reset'' (which works).
How Can it revert it back to how it was ? Did I mess up anything ? Does PA13 have to do with anything of this ??Thank you !!!2015-07-20 1:53 PM
PA13 is SWDAT, it's part of the debug interface.
Strap BOOT[0] High/VDD and erase the part with the ST-LINK Utilities. This will run the System Loader, instead of your code which immediate breaks the debugger's connection.2015-07-20 2:13 PM