2016-10-13 7:55 PM
I have an issue with a custom board using an STM32F427 that only shows up when I run outside the debugger. I've done some searching without any luck - is there a way to get TrueSTUDIO (or any other debug environment) to connect to a running board without issuing a RESET?
I'm running TrueSTUDIO v6 connecting to the target using the ST-Link v2 in SWD mode.
I've tried pre-starting the GDB_server in ''presistant mode'' and connecting to the ''remote'' GDB server from TrueSTUDIO .. but, when starting gdb_server, I get see:
C:\Program Files (x86)\Atollic\TrueSTUDIO for ARM 6.0.0\Servers\ST-LINK_gdbserver>ST-LINK_gdbserver.bat
Atollic TrueSTUDIO gdbserver for ST-Link. Version 2.4.3 Pro
Copyright 2010-2016, Atollic AB.
Starting server with the following options:
Persistant Mode : Enabled
LogFile Name : debug.log
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Connecting to the ST-Link Debugger...Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
ST_LINK Major version =2 Jtag version =25
ST_LINK VID=1155 PID=14152
ST_LINK device status: HALT_MODE
ST_LINK detects target voltage =3.21 Volt
Hardware watchpoint supported by the target
FuncEntry
STM32 device: id =20016419
STM32 device: Flash size =2048
FuncExit
FuncEntry
FuncExit
OK
Start Logging
Waiting for debugger connection...Waiting for TrueSTUDIO client to connect on port 61234 ...
I'm guessing that the ''Enter STM32_AppReset() function'' is probably what's doing it.
2016-10-14 9:49 AM
Hi kelly.andrew.001,
Try to update the ST-Link firmware to version V2-1 from the ST-Link utility (firmware update) or from this .-Hannibal-2016-10-16 3:16 PM
When I checked from ST-Link, there was a firmware update available .. so I updated.
No change though unfortunately, I'm still unable to connect without the target being RESET :(
2016-10-16 5:05 PM
Ok, well issues and setting with Atollic's ST-LINK GDB driver really need to be dealt with by Atollic and their support/settings. Disconnect the reset pin, try a J-LINK.
There might be a way to post-mortem a SWD connection, but there are better ways to pin these issues down. Have a USART connection, output telemetry, and have an effective Hard Fault Handler. Understand where you code is failing, the flow that got it there and where it might be crashing. The debugger configures the hardware it needs, make sure you enable the clocks you need. Describe the failure as currently seen.