2016-07-06 5:10 AM
1. how to set up
for fast
channel
change
2 .without recalibration
3. how to use
SDADC_CONF_INDEX_0
////////////////////////////////////////////////////////////////////////////////////////// ////////////////////////////CDADC///////////////////////////////////////////////////////////////////////////// /* Fill the SDADC handler with the parameters of initialisation */ /* An external reference is used. The other options are not used (low power, fast conversion,slow clock mode)*/ hsdadc1.Instance = SDADC1; hsdadc1.Init.ReferenceVoltage = SDADC_VREF_VDDA ;//!< The reference voltage is forced internally to VDDA */ hsdadc1.Init.IdleLowPowerMode = SDADC_LOWPOWER_NONE; hsdadc1.Init.FastConversionMode = SDADC_FAST_CONV_DISABLE; hsdadc1.Init.SlowClockMode = SDADC_SLOW_CLOCK_DISABLE; HAL_SDADC_Init(&hsdadc1); SDADC_ConfParamTypeDef confParam; ////////////////////////////////// /* -2- Prepare the channel configuration */ confParam.CommonMode = SDADC_COMMON_MODE_VSSA;// (SDADC_COMMON_MODE_VSSA 0v=8000)(SDADC_COMMON_MODE_VDDA 0v=8000) ; confParam.Gain = SDADC_GAIN_1;// SDADC_GAIN_1 0v=8000 5v=3967// SDADC_GAIN_2 0v=8000 5v=7FFF=+32767// confParam.InputMode = SDADC_INPUT_MODE_SE_ZERO_REFERENCE; confParam.Offset = 0x00000000; HAL_SDADC_PrepareChannelConfig(&hsdadc1, SDADC_CONF_INDEX_0, &confParam) ; //////////////////////////////////// HAL_SDADC_AssociateChannelConfig(&hsdadc1, SDADC_CHANNEL_1, SDADC_CONF_INDEX_0); HAL_SDADC_ConfigChannel(&hsdadc1, SDADC_CHANNEL_1, SDADC_CONTINUOUS_CONV_OFF); HAL_SDADC_SelectRegularTrigger(&hsdadc1, SDADC_SOFTWARE_TRIGGER); HAL_SDADC_CalibrationStart(&hsdadc1, SDADC_CALIBRATION_SEQ_1); HAL_SDADC_PollForCalibEvent(&hsdadc1, HAL_MAX_DELAY);//* Pool for the end of calibration *// ////////// HAL_SDADC_Start(&hsdadc1);//* Start regular conversion in polling mode */ /* Compute the input voltage */ HAL_SDADC_PollForConversion(&hsdadc1, HAL_MAX_DELAY);// /* wait for end of regular conversion */ TEST_U32 = HAL_SDADC_GetValue(&hsdadc1); ///////////////////////////////////////////////// #stm32f32016-07-11 2:55 AM
Hi novik.sergey,
Please, try to explain clearly your inputs here. If they are feedbacks/ bugs/ limitations or questions, you should mention that for each point. -Hannibal-2016-07-11 2:55 AM
Hi novik.sergey,
You'll probably want to review as many SDADC examples as you can find under STM32CubeF3 firmware: STM32Cube_FW_F3_V1.6.0\STM32Cube_FW_F3_V1.6.0\Projects\STM32373C_EVAL\Examples\SDADCTo have more details about SDADC, you can refer to this , section ''13 Sigma-delta analog-to-digital converter (SDADC) ''Hope this helps.Regards