2013-05-16 02:25 PM
Hi,
i'm reading the sensors on my STM32F3-discovery, and i've found out the reading arequite ''jumpy''. That means gyro and magnetometer value have consistent change (>1024) aven when the board is static. notice that accelerometer reading are fine. gyro and accelerometer are in sigle reading, and i chek the data ready bit (ZYXDA for gyro and acc, DRDY for magne) is set. BTW it still give me strange update frequency for sensor, like this bit is almost always set... I'm writing the reading over USB as audio USB card. here the output: [code] MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 MagZ diff: 1024.0 a:-16896.0 b:-17920.0 GyroY diff: 17495.0 a:17491.0 b:-4.0 GyroZ diff: 16621.0 a:16640.0 b:19.0 GyroY diff: -17477.0 a:14.0 b:17491.0 GyroZ diff: -16627.0 a:13.0 b:16640.0 read/sec:20963.831867057674 byte/sec: 179863.147605083 sensor read/s: giro 2783 acc 5110 magne 5206 different sensor read/s: giro 2783 acc 2783 magne 2476 [/code] and a peace of code, the part for gyro reding: [code] uint8_t Gyro_ReadAngRate (uint16_t* pfData) { uint8_t tmpreg; L3GD20_Read(&tmpreg,L3GD20_STATUS_REG_ADDR,1); if (!(tmpreg & 0x08)){ //no data ready! return 0; } int i =0; L3GD20_Read(buffer,L3GD20_OUT_X_L_ADDR,6); for(i=0; i<3; i++) { pfData[i]=(int16_t)(((uint16_t)buffer[2*i+1] << 😎 + buffer[2*i]); } return 1; } [/code]2013-08-23 09:06 AM
up?
2013-08-24 07:01 AM
One observation - the code uses unsigned 8 and 16 bit variables for gyro readings, the gyro produces 2's complement 16 bit values. That could explain the large jumps.
Cheers, Hal2013-08-27 09:37 AM
The supplied driver for this device says L3GD20_Read gets MS byte first, LS byte second. Are you processing the buffer bytes backwards ?
Cheers, Hal