cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F37x/STM32F0x I2C Timing Configuration Tool

gregg
Associate II
Posted on April 29, 2013 at 18:43

Hello everyone,

I'm writing to ask if anyone could provide a valid link to the STM32F37x/STM32F0x I2C Timing Configuration Tool which application note AN4235 refers to.  I've looked everywhere I know of on the site and I haven't been able to locate it anywhere.  The application note states:

'The configuration tool is implemented in the Microsoft Excel �I2C_Timing_Config_Tool_Vx.y.z.xls� file which can be downloaded from www.st.com.';

The application note is located on the main page for the part:

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1576/LN10/PF252209♯

This is ordinarily where I would expect to also find the related .xls file, but for the life of me I'm not finding it there, or anywhere else I've managed to look. 

Many thanks in advance for any time or efforts which can help me find this tool.

#amazing-google-skills #stm32f37x #cpal-i2c-stm32f0
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on April 29, 2013 at 18:49

http://www.st.com/web/en/catalog/tools/PF258335

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
gregg
Associate II
Posted on April 29, 2013 at 18:56

Thanks so much clive1!

I promise I'm as embarrassed about this as it warranted. 

edit:  I'm noticing now that It is listed for the stm32f0x series part, but not for the stm32f37x that I was looking at it for specifically.  I should have checked both.  Thanks again!

I don't know, it's not a tool I use.

I tend to read the RM and then build a fitter/solver tool based on the clocking/gearing described.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Mvill.17
Associate III

How to use it with OpenOffice?

There's an error in the macro.

Thanks