cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F373C8T6 Foot print and Symbol wrong Pinouts

vbakoti
Associate

I down load the STM32F373C8T6 Foot print and Symbol from STs website (Ultalibrarian)

But it has a wrong Pinouts connections (Pin numbers) 

VDD_2    Pin No.14

PA-4       Pin No 15

PA-5       Pin No 16

PA-6       Pin No 17

 

But actual connections are

PA-4.      Pin No 14

PA-5.      Pin No 15

PA-6.      Pin No 16

VDD_2.  Pin No 17     

 

Please observe this anyone designing with this foot print , and 

I Request ST to correct this foot print and Symbols 

 

 

1 REPLY 1
STTwo-32
ST Employee

Hello @vbakoti and welcome to the ST Community.

I confirm this typo and I've escalated to the concerned team for correction ASAP (under internal ticket number 201049).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.