cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F373 DAC Issue

Posted on July 06, 2018 at 11:20

The original post was too long to process during our migration. Please click on the attachment to read the original post.
2 REPLIES 2
AvaTar
Lead
Posted on July 06, 2018 at 11:56

Look up the datasheet - the DAC is too slow, with settling times of several microseconds.

The DAC output register throughput is less relevant.

Posted on July 08, 2018 at 11:37

AvaTar

Thanks for the reply. I checked the datasheet and it shows:

0690X0000060LhIQAU.png

Looks like I can update the DAC every 1 us but expect a settle time  up to 4 us when changing full scale 0 to 4095 ?