STM32F334, Use HAL lib to configure ADC with EXTI 11 as trigger + DMA
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-11-21 2:00 AM
Hi,
I'm trying to configure ADC2 to get data via DMA with external trigger interrupt.
I'm usign StCube framework.
I get read data via DMA with request capture via software with any problem, but I need to synchronise the external trigger with start ADC via HW (If i capture the external interrupt and after enable ADC, I have a big delay of 4us)
HAL_ADC_Start_DMA(&hadc2, (uint32_t*)buffDMA, 100)
But, I don't know how to start DMA when config EXTI
Here, code to config ADC with EXTI line 11
/* ADC2 init function */
static void MX_ADC2_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Common config
*/
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc2.Init.Resolution = ADC_RESOLUTION_8B;
hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc2.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_EXT_IT11;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DMAContinuousRequests = DISABLE;
hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc2.Init.LowPowerAutoWait = DISABLE;
hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
Now, how start device to get data via DMA when interrupt in EXTI_11 is fired?
Thanks
Jordi
Labels:
- Labels:
-
ADC
-
DMA
-
STM32F3 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0