2014-08-25 12:27 AM
New STM32F334 have high-resolution timer with 217 ps resolution,
It
's nice,
but
what
real
precision is achieved
when
the timer
used to measure the
time
between
two edges
of the signal applied
to
the processor
GPIO?
2015-03-18 1:58 AM
Hello,
The high-resolution is available solely for waveform generation. For input capture and period measurement, the external signals are resampled by the internal clock (144MHz). This corresponds to a 6.9ns resolution. What kind of resolution are you looking for? Is it for a single-shot (instantaneous) or multi-period measurement? Best regards, Vincent