cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F303RETx] I2C not working reliably with CAN enabled

ajaygargnsit
Associate II
Posted on July 12, 2018 at 17:07

Hi All.

We are using the MCU as the I2c-master, and a MPU6050 as the slave.

Following are the I2C-parameters of the MCU (from Cube) :

I2C Speed Mode                           :     Standard

I2C Speed Frequency (KHz)         :    100

Rise Time (ns)                               :    1000

Fall Time (ns)                                :     300

Coefficient of Digital Filter              :     0

Analog Filter                                   :     Enabled

Timing                                            :     0x00901D23

Slave Features

Clock No Stretch Mode                  :   Disabled

General Call Address Detection    :   Disabled

Primary Address Length selection :   7-bit

Dual Address Acknowledged         :   Disabled

Primary slave address                   :    0

I2C1_SCL is on PB6,  Open-Drain Mode, GPIO Pull-Up, Fast Mode Disabled.

Same for I2C1_SDA.

CAN is being used at 250 KHz, and it functions perfect, with both with/without I2C.

Now, when we use *only* I2C with CAN disabled, I2C's functioning is perfect.

We always get reply/data from MPU6050.

However, when CAN is enabled, I2C *almost* stops working.

I say *almost*, because spuriously we do get data, but 98% of times HAL_BUSY is returned while doing HAL_I2C_Master_Transmit.

One would tend to assume that I2C and CAN are different lines, so functioning of one would not be impacting another.

Unfortunately, I have been trying this for 2 weeks now, but no reliable solution has been achieved.

What could we further try?

Will be grateful for pointers.

Please let me know if I should provide any other information.

Thanks and Regards,

Ajay

#i2c-issue #stm32f303 #i2c-with-can
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0