2025-06-17 11:10 AM - last edited on 2025-06-25 3:31 AM by Amel NASRI
Hi all,
I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me!
Project setup so far:
Board: STEVAL-STWINBX1 (STM32U585AI MCU)
Using: Only the IIS3DWB vibration sensor (not the other sensors for now)
Peripherals: SPI2 (for IIS3DWB), UART2 (for debug/streaming), FreeRTOS
Goal: Read high-frequency vibration data, and eventually store it for later analysis
What I’ve tried:
I set up IIS3DWB via SPI2 and am running it at the full 26.7 kHz ODR (output data rate).
Because the data rate is so high, using an interrupt for every data-ready signal floods the CPU.
To handle this, I enabled the IIS3DWB internal FIFO (3KB, ~200 samples), set a watermark/threshold, and use the FIFO threshold interrupt to trigger reading.
My ISR releases a semaphore, which a FreeRTOS task then picks up to read out the FIFO using:
After that, I try to send the samples out via UART (just for testing), and I have another task blinking an LED to check if the CPU is getting starved.
The problem:
If I try to send all the FIFO data out via UART (using HAL UART transmit, not DMA), the FIFO quickly overflows and I lose data.
It seems UART can’t keep up with the sensor, and the rest of the system starts missing interrupts/tasks.
(Side question: Does iis3dwb_fifo_out_multi_raw_get automatically clear the read data from FIFO, or do I need to manually manage FIFO pointers or clear it after reading?)
What I want to try next:
Move all heavy data movement (sensor-to-memory, memory-to-UART) to DMA, so the CPU can handle higher-level logic and avoid being starved.
My idea is:
FIFO threshold interrupt fires → notifies a FreeRTOS task.
The task reads data out of the FIFO into a buffer (possibly with DMA, if supported).
Another task (or maybe same) sends the buffer out via UART using DMA as well.
I’m not 100% sure about the best way to architect this. My main goal is to reliably stream or store high-frequency sensor data without losing samples or overwhelming the CPU.
Questions:
What’s the best practice for moving high-rate sensor data from the IIS3DWB FIFO to UART or storage on this hardware?
Any gotchas with the DMA setup for SPI/IIS3DWB and UART on the STM32U5 series? Are there sample projects or HAL/LL code snippets for this?
For those with experience: Do I need to “clear” the FIFO manually after reading, or does the read function automatically pop the entries? (Can’t find this clearly in the docs.)
Any advice for task/interrupt/DMA priorities to make sure nothing is missed, especially as a beginner to FreeRTOS and STM32 DMA?
If you have working code, a block diagram, or even just advice on the pipeline, I’d really appreciate it!
I’m just a student, so I’m still learning a lot of the STM32 and sensor stack. If you spot any flaws in my thinking or have a more robust architecture, please let me know! Open to all suggestions, links, or example code.
My repository is: https://github.com/YumTaha/STWINBX1/tree/FIFO-Tasks
I track my learning there so I can always have it if I want to implement functions together
another thing I ran into is all the examples and help out there is mostly for other sensors rather than IIS3DWB, I couldn't find anything about this sensor.
Thanks so much!
2025-06-29 1:40 AM
I too started my own drivers and had discovered inconsistencies that don't seem to reflect the datasheet. Here's a ST driver for the IIS3DWB and some examples that were much more valuable to me than was the datasheet when it came to the firmware. STMems_Standard_C_drivers / iis3dwb_STdC at master · STMicroelectronics/STMems_Standard_C_drivers · GitHub