2017-02-04 7:00 PM
Hello
Is it possible to use dual interleaved mode with 2 different DMA channels in stm32f3?e.g one channel for adc1 master and another for adc2 (slave). there is some examples in stm32cube, using one dma channel.
Thanks.
2017-02-04 10:23 PM
After reading stm32f303 errata, it seems to be the limitation of mcu revision i'm using (stm32f3discovey and Y revision of the mcu) :
'
DMA overrun conditions can be encountered when two ADCs are working in dual
interleaved mode with a single DMA channel for both (MDMA[1:0]bits equal to 0b10 or
0b11). This limitation applies in Single, Continuous and Discontinuous mode.
'So what are the other revisions of this mcu available?