stm32f2xx interrupts working only in debug mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-06-02 04:29 PM
Posted on June 03, 2013 at 01:29
I'm trying to output vga signal using timer1 ch1 for hsync, ch2 for interrupt (horizontal backporch) and timer3 ch2 for vsync and ch3 for interrupt (vertical backporch). I'm using E0-E2 pins for direct output and I can get stable lines of colors, but only after I go into debug mode and run twice (after observing NVIC registers, they are blank and setup only after first run and active after second). Pins D12-D15 are used to signal the place in program (12 for end of main, 14 for tim3 interrupt and 15 for tim1 interrupt).
Here's the code:Don't know what else to try.Thanks for the help.P.S. I'm using Keil uVision and J-Link JTAG. #stm32-timer-interrupt-debug-mode
Labels:
- Labels:
-
TIM
0 REPLIES 0