cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207VGT6 VCP start fail

SimonLee
Associate II

Hi Mr. and Miss.
At present, I use a circuit board designed by myself, using STM32F207VGT6. Initialize the VCP function using STM32CubeIDE. But there was a phenomenon that it couldn't solve. Error Code10 displayed on Windows.

Attached is my circuit diagram and the settings of CubeIDE(Only initial setting without any code add or modified)

Where would this be causing the problem? Please give me some advice, much thanks.

SimonLee_3-1689243444127.png

SimonLee_4-1689243461469.png

SimonLee_0-1689243578526.png

 

 

SimonLee_2-1689243335525.png

 

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Piranha
Chief II
Update Windows Forms 10 to 11.

https://en.wikipedia.org/wiki/Windows_Forms

Less nonsense would help... And the proper solution is tossing out the broken bloatware and using, for example, this:

https://github.com/hathach/tinyusb