2011-09-21 8:35 AM
Hello everyone. This is my first time posting here and I am having issues with the IAP found here at STM's website. I am using Rowley Crossworks and the IAP files do not support that. Instead I created my own project and got the bootloader to run fine using USART communication. The first problem I ran into was when downloading my *.bin blinky program in FLASH_If_Write when it checks the data written to flash it was coming back and saying it did not match the SRAM content. I commented this out and was able to upload my whole bin file. If I look where blinky was written the code looks 100% fine. I am writing to 0x08008000 and my bootloader is at 0x08000000. I made sure the code doesn't overlap.
Now my real issue is jumping to the blinky application. The code sequence JumpAddress = *(__IO uint32_t*) (APPLICATION_ADDRESS + 4); /* Jump to user application */ Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) APPLICATION_ADDRESS); Jump_To_Application(); Jump address ends up pointing to location 0x08000351 and my debugger just goes to DEFAULT_ISR_HANDLER reset_wait in startup.s. Now I know my blinky app works as I tested stand alone. Two questions: While debugging should I expect the blinky app the execute after the jump? Has anyone experienced this or can provide an insight to what the issue maybe? Thanks in advance and sorry if anything I posted is confusing this is my first technical post.2011-09-23 8:37 AM
The odd address infers that it's calling Thumb code (Cortex-M3 can't run 32-bit ARM code)
Calling 0x08008004 will not work, it's a vectoring address not an instruction. Further, as an even address the core thinks it's ARM code, and will trap. The value at 0x08008004 points to 0x08000351, which suggests that the code is not compiled/linked correctly for a basis of 0x08008000 which you need for your application image. The vector should point to the c startup code, which should set up the stack, move/clear the static segment, set the stack, then call main(). I need to dig up my 1.6/1.7 licence, and try the 2.x eval2011-09-23 8:58 AM
Clive,
A little update. I defined STARTUP_FROM_RESET in my blinky project and it now appears that 0x08008004 has the address of the reset_handler ( 0x080000289). Still end up at the hardfault handler and I will see what I can figure out. Thanks again.2011-09-23 9:31 AM
Looks like it's still pointing back into the Boot Loader region, and not the Application region.
A quick look at one of the 1.6 linker scripts (.ld) You'd need to shrink the FLASH size by 0x8000 (32KB), and advance the base, at all places it's specified. You'd need to expand the __STACKSIZE__ to reflect the application's needs. MEMORY { UNPLACED_SECTIONS (wx) : ORIGIN = 0x100000000, LENGTH = 0 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 0x00080000 SRAM (wx) : ORIGIN = 0x20000000, LENGTH = 0x00010000 USB_CAN_RAM (wx) : ORIGIN = 0x40006000, LENGTH = 0x00000200 CM3_System_Control_Space (wx) : ORIGIN = 0xe000e000, LENGTH = 0x00001000 } SECTIONS { __FLASH_segment_start__ = 0x08000000; __FLASH_segment_end__ = 0x08080000; __SRAM_segment_start__ = 0x20000000; __SRAM_segment_end__ = 0x20010000; __USB_CAN_RAM_segment_start__ = 0x40006000; __USB_CAN_RAM_segment_end__ = 0x40006200; __CM3_System_Control_Space_segment_start__ = 0xe000e000; __CM3_System_Control_Space_segment_end__ = 0xe000f000; __STACKSIZE__ = 128; __STACKSIZE_IRQ__ = 0; __STACKSIZE_FIQ__ = 0; __STACKSIZE_SVC__ = 0; __STACKSIZE_ABT__ = 0; __STACKSIZE_UND__ = 0; __HEAPSIZE__ = 128; ....2011-09-23 10:35 AM
With 2.1 I created a custom ''Memory Map File'' in the project directory
ie $(ProjectDir)/STM32F207IG_MemoryMap_App.xml and associated the project option ''Memory Map File'' with it instead of the default one. And replaced the last line <MemorySegment size=''0x100000'' access=''ReadOnly'' name=''FLASH'' start=''0x08000000''/> with <MemorySegment size=''0xF8000'' access=''ReadOnly'' name=''FLASH'' start=''0x08008000''/> The original file will be installed wherever you put the packages, for example C:\Users\YourUserNameHere\AppData\Local\Rowley Associates Limited\CrossWorks for ARM\packages\targets\STM32\STM32F207IG_MemoryMap.xml Now the map file looks like this : ... Memory Configuration Name Origin Length Attributes UNPLACED_SECTIONS 0xffffffff 0x00000000 xw FLASH 0x08008000 0x000f8000 xr RAM 0x20000000 0x00020000 xw SRAM1 0x20000000 0x0001c000 xw SRAM2 0x2001c000 0x00004000 xw BKPSRAM 0x40024000 0x00001000 xw PCCARD 0x90000000 0x00000000 xw NAND2 0x80000000 0x00000000 xw NAND1 0x70000000 0x00000000 xw NOR_PSRAM4 0x6c000000 0x00000000 xw NOR_PSRAM3 0x68000000 0x00000000 xw NOR_PSRAM2 0x64000000 0x00000000 xw NOR_PSRAM1 0x60000000 0x00000000 xw CM3_System_Control_Space 0xe000e000 0x00001000 xw *default* 0x00000000 0xffffffff Linker script and memory map 0x08009044 __do_debug_operation = __do_debug_operation_bkpt 0x08008368 __vfprintf = __vfprintf_int 0x08008ad4 __vfscanf = __vfscanf_int 0x08008000 __FLASH_segment_start__ = 0x8008000 0x08100000 __FLASH_segment_end__ = 0x8100000 0x20000000 __RAM_segment_start__ = 0x20000000 0x20020000 __RAM_segment_end__ = 0x20020000 0x20000000 __SRAM1_segment_start__ = 0x20000000 ... .init 0x08008184 0x1dc 0x08008184 __init_start__ = . *(.init .init.*) .init 0x08008184 0x104 THUMB Debug/thumb_crt0.o 0x08008184 _start 0x08008202 exit .init 0x08008288 0xd8 THUMB Debug/STM32_Startup.o 0x08008288 reset_handler 0x0800829a SystemInit ... Bit of a pain, but not too hard to do.2011-09-23 10:50 AM
Clive thanks again for your help! I modified the linker file in my blinky project to have flash start at 0x08008000 and this fixed my issue! I cannot thank you enough for your help!!!
I will modify the xml to be included in my real project! Thanks, Brad