cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207 Nucleo 144 UART1 Baud Rate

sumit kale
Associate III
Posted on January 23, 2017 at 14:57

Hello,

i want a baud rate of 5 mbps on UART1/UART6 on STM32F207 Nucleo Board (As per reference Manual UART1 & UART6 can have baud rate up to 7.5 Mbps). However when i am configuring in STM Cube MX i am getting baud rate of 3.7 mbps max for both UART1 & UART6. I have checked clock configuration many times.

HCLK= 120 MHz, APB1= 30MHz, APB2=60 MHz exactly. In Addition to this i also tried to give Input frequency of 25MHz (26 MHz max).

Still i am unable to cross 3.7 Mbps (max possible value as per Cube Mx)

So can anybody suggest me possible solution??.

#stm32f207-uart
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on January 23, 2017 at 16:15

Thank you..Got it..