STM32F205ZGT7 - Need technical support to program the STM32 in the OTA(On-The-Air)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-21 7:57 AM
Hi, Thanks for sharing the experience and timely support.
I am new to STM32 controller and OTA programming. Kindly share the suggestion for the below queries.
Environment - STM32F205ZGT7, IAR workbench, ST-Link V2
1) Which executable file(.hex,.out,.bin) need to be used for OTA programming?
2) Suggestion for format(example - Motorola S-record) need to be followed to transmit the program file in the OTA and suitable for error recovery? (Info : executable file is available in the Cloud Server)
3) Executable file Received OTA need to be stored in the external flash and then during the restart custom boot-loader need to fetch the executable code from the SPI flash and write to the internal flash. (Info : custom boot-loader and Application program will be developed as a independent IAR workbench project).
Currently I need to develop the test application that perform the internal flash programming using the executable code stored in the SPI falsh. So I required to store the executable file in the test application code. So Which executable file(.hex,.out,.bin) need to be used and how to use it?
- Labels:
-
STM32F2 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-21 8:16 AM
The air doesn't really care what format you use, a binary format would be the most efficient. I'd probably use a packaged binary for that is compressed, encrypted and signed.
The DFU format might provide more modes of deliver, it is a binary format, allows for sparse files, and has a CRC. You could deliver via USB, SD Card, or whatever.
Review IAP (In-App Programming) examples.
Up vote any posts that you find helpful, it shows what's working..