2014-02-23 7:42 AM
2014-02-23 9:47 AM
What does not work?
http://en.wikipedia.org/wiki/Moving_average
We describe some possible formulas
I used the moving average window
You need to store N consecutive samples where N is the width of the window
The average value is
Mn +1 = Mn - sample (n - N) / N + sample (n +1) / N
or in the best form
N * Mn +1 = N*Mn - sample (n - N) + sample (n +1)
and divide by N only when necessary. (But you must be careful N*Mn must be stored in 32bit ma
x) In other words, remove from the average the buffer oldest value and add the last measureSample data buffer can be implemented with a circular buffer.
( last measure replaces the oldest value and you can easily calculate the above formula )
At powerup
fill ALL the data buffer with
the first A/D measure (This prevent the startup delay caused by average )If possible, for evrey measure exec multiple high speed A/D conversions and
performs the average of these measures
Normally I exec 10 high speed A/D conversion I subtract the min and the max values and I shift right 3 time (8 divide) the results
This value is my new sample.
ks..2014-02-23 4:42 PM
Thanks for explanations... and wiki link.. but not solved the problem
2014-02-26 5:17 PM
Hello Diego,
In terms of functions, interrupts and config things.. Did you have any example to show?In my codes i divide the buffer on two parts:The newest and the oldest part...When the interruptions (HT or TC) are called the other half of buffer is subtracted and current part is added. (see the interruption of DMA)I stored a certain amount of data and then do the calculations .. The initial values are correct but after some time the values begin to show errors. If the input voltage varies widely the error is even greater. Even though I keep constant signal after a large variation results are never consistent. Only resetting the module restore the correct values of average.Tkz...2014-02-27 12:05 AM
germanovix
for me it is impossible to find a problem just by reading some of the code without debugging support
I would do this:
Control the number and sequence of the DMA interrupt eg using counters that increments on flags HT and CT ( If you lose a few interrupts as you see it )
Control of the data buffer .
I would use only two input values (eg two batteries 1.2V and 2.4V ) each time you fill a buffer check that all the values are correct .
Start acquisitions test at very low frequency to verify interrupt dma etc.
If you have free ram created a temporary buffer where download all
acquired
data, or if possible send buffer to serial portI do not know if there is an error in the calculations but to do a test: create a know data buffer (ex a ramp) calculate the moving average for te know buffer and save all the results in another buffer
Remove the DMA transfer and work with conversion complete interrupt Another test add increment counter in DMA interrupt anddecrement counter when data is processed
When you start buffer processing the counter value must be 1 (not > 1)2014-02-28 1:17 AM
The initial values are correct but after some time the values begin to show errors. If the input voltage varies widely the error is even greater.
Even though I keep constant signal after a large variation results are never consistent. Only resetting the module restore the correct values of average. Sounds to me like an overflow in your calculation. However, I suggest to separate your issues. Pull your moving-average implementation/functions out and test them on a PC. I'm using the CodeBlocks IDE for such purposes. This lets you feed the algorithm with simulated input data, watch the intermediate results in the debugger, and verify it. Only then I would go on to check if the input data feed (ADC/DMA) is correct.