Associate II
December 13, 2011
Question
STM32F10xx two USART at the same time
- December 13, 2011
- 2 replies
- 755 views
Posted on December 13, 2011 at 13:23
Hello,
Pardon by my english. I need two USART work at the same time. One USART is all the time sending bytes and the other USART is receiving bytes.I work with USART configures in Half Duplex mode. I work in baudrate of 7200bps. I have changed the priority of the NVIC, first both USART with the same priority and next one with higest priority. In the attach file, I put the code with which I configure both USART. My problem is that I lose bytes. Is my configuration wrong?