2014-01-16 12:00 AM
I use STM32F103 in a project which is hard to access device after installation. Also it is manufactured in large quantity. I can get a serial port access to the out of device for updating firmware of device in future, but device is completely close and it is not possible to change status of BOOT0 & BOOT1 for entering system memory boot mode.
Is there any USART bootloader to use in STM32f103 which use to update device's program without changing status of MCU pins? Regards, Thanks,2014-01-21 06:41 AM
2014-01-25 07:03 AM
Fatemeh
Give your email for IAP help.(design your own bootloader). Regrads2014-01-26 04:56 AM
fatemeh.jamali@yahoo.com
Thanks,