2017-09-03 8:42 PM
HI.
Currently I'm trying to understand about STM32F10x's interrupt.So I've got some snippet code as the below,USART1's IRQ number is 37.
// interrupt example snippet code //
unsigned int vector_table_start_addr = *(unsigned int *)0xE000ED08 ; // VTOR register OK.*(unsigned int *)(vector_table_start_addr + (16+37)x4 ) = UART_Handler; // cf) UART_Handler set ??
*(unsigned char *)(0xE000E400+37) = prio;
unsigned int offset = (unsigned int)(37/32)*4; unsigned int bitpos = (unsigned int (37%32); *(unsigned int *)(0xE000E100+offset) &= ~(1<<bitpos);Q1. what does (16+37)x4 mean in *(unsigned int *)(vector_table_start_addr + (16+37)x4 ) = UART_Handler; ??
Would you please let me know how does it come from? and how to understand it?Q2. How does it get
0xE000E400 and 0xE000E100 address number from *(unsigned char *)(0xE000E400+37) = prio; and
*(unsigned int *)(0xE000E100+offset) &= ~(1<<bitpos);
Would you please let me know how does it come from? and how do I understand it?
#stm32f1x-interrupt2017-09-03 9:16 PM
There are 16 slots for 'System Handlers' which are generated via the SCB, the remaining interrupts are generated via the NVIC. The NVIC design maximum is 240 interrupts. ie 240+16 = 256
Each 32-bit register is 4 bytes wide, this is where the *4 comes from. The USART1 interrupt is number 37, and has to index past the 16 system handlers in the vector table, thus the addition.
Look at a listing file when assembling the startup_stm32f10x.s file
The priority registers in the NVIC are 8-bit wide, the USART1 priority is 37 bytes into the priority register array.
The 37/32 gets you an offset into a 32-bit register file, the *4 gets you from a byte index to a word index, the bitpos 37%32 gets you a bit position within the selected 32-bit register holding the enable bit.
Look at the NVIC documentation in the ARM Technical Reference Manual for the Cortex-M3, understand the bit, byte and word representation of registers with the processors address space.
The example assumes the vector table is in RAM
2017-09-04 2:18 AM
Hi Clive,
I came across the below such as Interrupt Set-enable Register.
and There are 8 Interrupt set-enable registers NVIC_ISER0~7.
But I'm wondering what if I want use interrupt function then should I have to choice the one of 8 registers?
How can we know which NVIC_ISERx should we have to use?