STM32F107VC AND KEIL PROBLEM
Hello ;
I am new to STM32 ; right now I could blink a led I have good experience with other MCU venders ; but this first time to ARM. I have strange problem with my code ; when I dont use the routine creatfile(); the program work as expect ; but when i add them to the code the program first get : NMI_Handler and then stuck some place .. the code is here : GPIO_InitTypeDef GPIO_InitStructure;// void creatfile(void) ;
//-- void init_card (void);void delay(unsigned int time) {
while(time--);
}volatile unsigned int delay_main;
//-------
//------------
int main(void) { /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f10x_xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f10x.c file */ //RTC_NVIC_Configuration();/* system Tick enable timer----------------------- */
SystemCoreClock =72000000 ; if(SysTick_Config(SystemCoreClock / 1000)) // 1 ms interrupts while(1); // error /* GPIOD Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE);/* Configure PD0 and PD2 in output pushpull mode */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_SetBits( GPIOD, GPIO_Pin_3 | GPIO_Pin_4);//-----------------
init_card ();
//creatfile();
// while(1) { GPIO_SetBits( GPIOD, GPIO_Pin_3 | GPIO_Pin_4);while (delay_main<1000); delay_main=0; GPIO_ResetBits( GPIOD, GPIO_Pin_3 | GPIO_Pin_4); while (delay_main<1000); delay_main=0; }
init_card ();
}void init_card (void) {
U32 retv;while ((retv = finit (NULL)) != 0) { /* Wait until the Card is ready*/
if (retv == 1) { while(1); } else { } } }void creatfile(void) {
char *fname, *next; FILE *f; int i,cnt = 1000;f = fopen (''ASSAAD.TXT'', ''w''); /* open a file for writing */
if (f == NULL) { while(1); return; } for (i = 0; i < cnt; i++) { fprintf (f, ''This is line # %d in file %s\n'', i, ''ASSAAD.TXT''); } fclose (f); /* close the output file */ while(1); } //--------#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) *//* Infinite loop */
while (1) { } }#endif
/**
* @} *//**
* @} *//******************* (C) COPYRIGHT 2011 STMicroelectronics *****END OF FILE****/
Thank you Regards