2010-03-28 2:01 AM
STM32F105 need usb mass storage demo + SDIO
2011-05-17 4:44 AM
Hi Alexander
I search USB example for STM32f105 tooand I don't find sources. What did you find about mass storage ? I need USB host example to load files from mass storage. Can you give me sources you found or say me where you found it ? Thanks2011-05-17 4:44 AM
''I found very good examples of USB mass storage in IAR's example folder but for STM32F103 only''
So what's stopping you just using that on the STM32F105 ??2011-05-17 4:44 AM
I found here:
''C:\Program Files\IAR Systems\Embedded Workbench 5.** Evaluation\ARM\examples\ST\STM32F10x\IAR-STM32F103ZE-SK\MassStorage\''
It is example of USB Mass Storage Device only (for F103 chip).. As I see you need something else2011-05-17 4:44 AM
USB of 105/7 very differ whith 103. Every other modules works fine on 105 exept USB.
I dont have so much knoleges to port USB-MSD code from 103 to 105... maybe someone did it already?
2011-05-17 4:44 AM
Hi,
I think the best way is that you take spi SD card driver provided by STM32stdFWLib (http://www.st.com/stonline/products/support/micro/files/stm32f10x_stdperiph_lib.zip
, under the folder: STM32F10x_StdPeriph_Lib_V3.2.0\Utilities\STM32_EVAL\Common\stm32_eval_spi_sd.c/h). and you implement it in the Mass Storage demo. Is this the kind of information you are looking for or do you need help in implementing the code ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.