2013-01-18 8:35 AM
Hello all,
I am working on a project where I need to implement USB mass storage device. My SD card is communicating with controller on SPI2. As this microcontroller doesn't have the library for SPI so I used library code from STM32F103VBH6(eval board). But after integrating the code with my application I never get the device configured.I am new to USB don't know how to go with it. My USB is running at 48MHz. and SPI at 400KHz. D+ is permanently pulled high with 1.5k resistor.Do I need to make any changes needs to be done in the code.
Please let me know where I am gone wrong.Thanks in advance. #stm32f103-usb-msd